cancel
Showing results for 
Search instead for 
Did you mean: 

Cube Ecosystem - A Rant

lryfer
Associate II

For years, ST seems to spit in the face of developers every time they try to “improve” the ecosystem. Even now they’re trying to move toward *** like AI chips or other *** that sounds great to shareholders, while we developers are left with the crumbs of their work. These chips are widely recognized around the world and probably have some of the best engineers in the industry behind them, and yet what we actually get as developers are slow programs programs with a thousand issues on Linux, badly developed no matter how you look at it.

Recently, as Linux programmers, we ran into the problem that CubeProgrammer was using an “hack” I can’t call it anything else where it used an sprintf() on stdin to try to catch all files starting with 0x*. And as soon as this recursive hack stopped working, they blamed Linux for the issue (obviously). All these applications are written in Java and are ridiculously slow, to say the least. An Eclipse-based IDE in 2025 feels like a slap in the face to anyone who wants to produce good software but is dragged down by terrible support that the developers don’t really provide.

Let’s talk about the big problem: CubeIDE. This is supposedly the only “clean” way to work on projects, and it’s the real pachyderm of embedded development. On top of the constant workspace breakages across all platforms, this IDE is nearly unusable. The pseudo LSP barely works, errors are not runtime, there’s no flychecking, and we’re stuck using ***py build systems that aren’t even modern. And honestly, as a developer, I don’t even want a “better Eclipse.” I just want to stop using it. The debugging works well no complaints there but there are simply no real alternative ways to work decently with these poorly maintained products.

HAL often has problems too, and we developers end up touching CMSIS which I guess is the standard for Cortex-M but we’ve truly reached the limit. The development environments need real improvement. And the one they made for VSCode is not an alternative. Maybe ten people use it. And if ST’s developers actually used it themselves, they wouldn’t ignore the fact that it’s full of bugs, integrates poorly, doesn’t genuinely meet developers’ needs, and whenever you start a project you usually have to manually hack together debug integrations because the official one is half baked. At that point you might as well use OpenOCD, which is more stable. BUT everything becomes unstable again the moment you open CubeMX to regenerate the project.

On top of this, CubeMX can generate CMake and Makefiles, which is basically the only sane way to write software in 2025. Most editors need the generation of a CMakeLists.txt, and ignoring this is genuinely *** and counterproductive to the company’s own interests. And since I do everything in nvim and VSCode, it seemed like the only escape from that horrible “IDE” nightmare.

The fact that the CMake option is semi hidden, that ST doesn’t advertise it, and doesn’t even integrate it into the IDE infuriates me, because ST is clearly trying to lock developers into the IDE and avoid giving any way for anonymous project data not to be collected. Then CubeMX doesn’t generate any clean way to compile, flash, or debug. It basically dumps the HAL files with the configuration you asked for and says, “okay, now you handle everything else.” And using comment markers inside files as generation points in 2025 is comica but that’s a rant for another day.

I hate how ST occasionally throws us a “little treat” to keep us quiet, and as a developer this is painfully obvious. I hate how “enterprise” the choice of including an ST microcontroller in your project has become. Because choosing a microcontroller is a choice, and it shouldn’t force you to change your entire toolchain just to accommodate a microprocessor manufacturer even if, being Italian, we’re practically forced to use this giant’s chips.

So I ask ST: do you really want to keep going in this direction? Can’t you create generic tools that let every developer work the way they want, in the best possible way, with the stability that a giant should guarantee? Don’t you want to allow external debugging, or the ability to write real, functional configurations or plugins? Don’t you want to contribute even a little to open source, letting developers expand your ecosystem and make it amazing?

Because what you’ve done or what you did once was great, but we can’t keep praising what was built in the past, especially when the ship we’re sailing on is full of holes. Especially when fixing that ship requires just the minimal effort of not being so greedy, and when all you really need to do is throw out that pachyderm of an IDE and build a clean, universal toolchain without excessive telemetry, without bloatware, extensible, fair for everyone, possibly open, and worthy of the best developers embedded has.

And this isn’t about closing doors I want to open every door possible. I want ST’s developers to cooperate and respond to all these questions. I want consumers (us) to participate and express our opinions with the guarantee of remaining partners of this company (ST) and continuing to build amazing things but starting to do it without constantly smashing our heads against the wall.

I believe we can do it, and I hope that everything I’ve expressed won’t be deleted just to protect the company’s image, but instead can start a conversation that actually improves my life as a developer and the lives of many others.

10 REPLIES 10
mbarg.1
Lead

I fully share the frustration working with ST - dozen of bugs submitted - no reply - or even worse, getting a f2f reply " we have to sell chips, sw is just some extra, take as it is or go somewhere else".

I stay hopefull that some day someone in ST will understand that sucessful solutions does need good sw beyond good hw.

While you have some good points I disagree marking this post as a bug report. It's not. It's a rant without any specific issue that can be reproduced and solved.

STM32CubeMX is flawed, but bugs are fixed. The forum is helpful with helping people to solve problems. It's up to users to test and verify code. I'm happy with it.

For quite some time I've been dreaming about designing an alternative to STM32CubeMX. I would do many things differently:

  • Code generation would still be an option, but I would also make an alternative: data-based initialization without conditional compilation or generated code. Just a struct with all parameters needed to initialize a peripheral. This would allow changing peripheral configurations while debugging easier. It would also simplify unit tests.
  • I would also allow multiple (sub)configurations so you can have board version dependent peripheral configurations or switch your device to different modes. Right now re-configuring a peripheral is a nightmare.
  • I would make it completely command line based, but with a gui based on wxwidgets, which is fast and portable
  • the project file (.ioc equivalent) would be more merge friendly. Right now ioc files are impossible to merge in git. Too many things are put on one line and adding one thing can change unrelated lines because numbers are inserted.
  • I would support different build systems in addition to CMake such as Meson and perhaps even Python scripts
  • I would reduce the number of macros in driver code or get rid of all of them
  • I would support adding custom user code sections.

 

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.

you are right, It's in bug report for a mistake, thank you to pointing that out


@lryfer wrote:

you are right, It's in bug report for a mistake, thank you to pointing that out


Removed "Bug-report" tag from the post

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

thanks!!!!


@unsigned_char_array wrote:
  • I would also allow multiple (sub)configurations

I would find that really useful!

 


@unsigned_char_array wrote:
  • the project file (.ioc equivalent) would be more merge friendly. Right now ioc files are impossible to merge in git. Too many things are put on one line and adding one thing can change unrelated lines because numbers are inserted.

Absolutely! This is a right pain!

TBF, this is not unique to Cube: many other IDEs have project formats which are hostile to merge/diff - even lines get reordered at random!

 


@unsigned_char_array wrote:
  • data-based initialization without conditional compilation or generated code. Just a struct with all parameters needed to initialize a peripheral. This would allow changing peripheral configurations while debugging easier. It would also simplify unit tests.

Not sure what you mean by that - the initialisations are largely struct-driven already ?

 


@unsigned_char_array wrote:
  • I would reduce the number of macros in driver code or get rid of all of them

Not sure what you mean by that?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Andrew Neil wrote:

@unsigned_char_array wrote:
  • data-based initialization without conditional compilation or generated code. Just a struct with all parameters needed to initialize a peripheral. This would allow changing peripheral configurations while debugging easier. It would also simplify unit tests.

Not sure what you mean by that - the initialisations are largely struct-driven already ?

Take, for example, GPIO (MX_GPIO_Init):

  1. GPIO_InitStruct is a local variable that is initialized with literals and repeatedly overwritten. It's not a const/constexpr that can be passed to a unit test or switched when changing hardware or mode. There is not even a user code section in that function to override it. They might as well have generated direct register write operations in that function and make that function inline.
  2. the line __HAL_RCC_GPIOX_CLK_ENABLE() is added when a GPIO port, that is not by default initialized, is used. It's not in the struct. If configuring pins at run time, for instance when checking board version or switching mode, I want it to dynamically enable/disable this clock.

Right now I use macro tricks to overwrite generated functions such as MX_GPIO_Init to make them board version depended.

 


@Andrew Neil wrote:
@unsigned_char_array wrote:
  • I would reduce the number of macros in driver code or get rid of all of them

Not sure what you mean by that?


This is less about the generated code, but more about the HAL. That heavily relies on macros. In C++ you cannot typecast a pointer to an address in constexpr (see this video for an example: https://www.youtube.com/watch?v=zBkNBP00wJE). Also some function like macros can be replaced with static inline functions or constexpr. 

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.
TDK
Super User

> The fact that the CMake option is semi hidden, that ST doesn’t advertise it, and doesn’t even integrate it into the IDE infuriates me, because ST is clearly trying to lock developers into the IDE

Yeah, I don't think they care, particularly. How is it hidden? The default toolchain isn't even STM32CubeIDE which doesn't lend much credibility to this argument.

Commercial options exist if you don't like CubeIDE.

 

> Because what you’ve done or what you did once was great, but we can’t keep praising what was built in the past, especially when the ship we’re sailing on is full of holes.

The CubeIDE and HAL software is the best it's ever been. It's not perfect, but it has been on a steady upward trajectory over the past 5 years. I am unconvinced the bizarrely named "STM32CubeIDE for VSCode" will ever get there, but we will see.

If you feel a post has answered your question, please click "Accept as Solution".
LCE
Principal II

It seems I'm quite lucky coming from the hardware side, having learned assembler (8-bitters, and mostly forgotten...) and C firmware on the job. :D

So I'm more happy about the inexpensive Nucleo-boards and the free tools than I am abhorred by the SW they deliver - using HAL / LL only when it doesn't matter (or isn't too "bad").

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.