2015-12-10 12:40 AM
Hello
I have a nucleol152 board. As I need to protect a memory area, I used this function to make a read protection + a write protection on zone specific areas:__IO uint32_t WPR_Value = 0x0, WriteProtectedPages = 0x0;
FLASH_Unlock(); /* Unlock the Option Bytes */ FLASH_OB_Unlock(); /*Set read protection to 1*/ FLASH_OB_RDPConfig(OB_RDP_Level_1); /* Get pages write protection status */ WPR_Value = FLASH_OB_GetWRP(); /* Get current write protected pages and the new pages to be protected/unprotected */ WriteProtectedPages = (WPR_Value & FLASH_PAGES_TO_BE_WRITE_PROTECTED); /* Check if desired pages are not yet write protected */ if(WriteProtectedPages != FLASH_PAGES_TO_BE_WRITE_PROTECTED) { /* Enable the pages read/write protection */ FLASH_OB_WRPConfig(FLASH_PAGES_TO_BE_WRITE_PROTECTED, DISABLE); /* Generate System Reset to load the new option byte values */ FLASH_OB_Launch(); } /* Lock the Option Bytes */ FLASH_OB_Lock();When I try to reflash my board using the stlink, I have a fail. I understand it fails as memory is protected.
I tried several things to unblock the memory: I use GDB to write the following sequence unlock flash (gdb) set {int}0x40023C10 = 0x8C9DAEBF (gdb) set {int}0x40023C10 = 0x13141516 unlock OB (gdb) set {int}0x40023C14 = 0xFBEAD9C8 (gdb) set {int}0x40023C14 = 0x24252627 switch to RDP level 0 (gdb) set {int}0x1FF80000 = 0x000000AA This last operation always fails and GDB returns that it cannot access to this memory area. I tried to push this sequence into a RAM program but it still has no effect (unless the code I downloaded is not working well). I saw this type of topic and I was wondering if it was the only solution to unblock my memory. http://www.mobilewill.us/2015/06/stm32-nucleo-and-dfu-usb-bootloading.html Could you tell me how I should proceed to unblock the memory? Thanks for your support #rdp #nucleo #st-link #swd2018-06-01 2:37 AM
Hey are you getting a solution of this issue??
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.