2021-04-02 5:08 AM
Here is the report:
Open On-Chip Debugger 0.11.0-rc2+dev-00037-g4c4dbd9 (2021-02-09-13:39)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J37S0 (API v2) VID:PID 0483:3748
Info : Target voltage: 2.903249
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L152RCTx.cpu: hardware has 6 breakpoints, 4 watchpoints
Info : starting gdb server for STM32L152RCTx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : stlink_dap_op_connect(reconnect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L152RCTx.cpu: external reset detected
Info : accepting 'gdb' connection on tcp/3333
Info : Device: STM32L1xx (Cat.3 - Medium+ Density)
Info : STM32L flash size is 256kb, base address is 0x8000000
Warn : GDB connection 1 on target STM32L152RCTx.cpu not halted
undefined debug reason 8 - target needs reset
Info : stlink_dap_op_connect(reconnect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L152RCTx.cpu: external reset detected
Info : stlink_dap_op_connect(reconnect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L152RCTx.cpu: external reset detected
Info : stlink_dap_op_connect(reconnect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L152RCTx.cpu: external reset detected
Info : stlink_dap_op_connect(reconnect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L152RCTx.cpu: external reset detected
Info : stlink_dap_op_connect(reconnect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L152RCTx.cpu: external reset detected
Info : stlink_dap_op_connect(reconnect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L152RCTx.cpu: external reset detected
Info : stlink_dap_op_connect(reconnect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L152RCTx.cpu: external reset detected
Info : stlink_dap_op_connect(reconnect)
Info : SWD DPIDR 0x2ba01477
Info : STM32L152RCTx.cpu: external reset detected
Info : accepting 'gdb' connection on tcp/3333
Warn : GDB connection 2 on target STM32L152RCTx.cpu not halted
undefined debug reason 8 - target needs reset
undefined debug reason 8 - target needs reset
shutdown command invoked
Info : dropped 'gdb' connection
shutdown command invoked
2021-04-02 6:12 AM
You have something else attached to the NRST line?
There is a Watchdog executing in your code, or prior code.
There is a POR circuit detecting low voltage. Check VDDA
2021-04-02 9:41 AM
You have something else attached to the NRST line? Nothing Attached, Stable 2,85V
There is a Watchdog executing in your code, or prior code. No watchdog executed
There is a POR circuit detecting low voltage. Check VDDA. Stable 2.95V
When I copy from:
everything works just fine, but when I use the STM32Cube device tool configurator to create code, then it doesn't work.
2023-12-08 4:41 AM
I have run into a similar problem using the same micro. Were you able to resolve the problem? What was the fix?
2023-12-08 4:49 AM
Custom board? Some code works fine, but others cyclically reset?
Check clocking expectations, input clock, HSE_VALUE, PLL settings.
Perhaps comment out code switching to HSE/PLL and let continue with MSI/HSI default.
2023-12-08 5:12 AM
I am using a custom board. Nothing else is on the NRST line. NRST is pulled to Vcc through a 10k resistor. The program will execute up to 500 lines of code before getting an external reset. Using HSI, not HSE. Configuration code was generated using STM32CubeIDE. I have stripped the application code down to just a loop and counter.
2023-12-08 10:16 AM
Using a WatchDog ?
Simple LED / GPIO toggle in main(), basically just initialize the pin, drive high / low, and scope pin does that crash? Avoid calling HAL_Init(), SystemClock_Config(), etc. Keep it simple.
Supply droops? POR/BOR settings in Option Bytes? NRST pulses lows? scope
Provide a schematic of salient connections to STM32. Going to be hard to diagnose without some detail.
VDDA/VSSA connected to supplies
2023-12-09 9:11 PM
I did as you suggested and simplified my code. With calls to HAL_Init and SystemClock_Config() removed and the software simply toggling an output, I do not experience any external interrupts. When I call HAL_Init or SystemClock_Config() an external interrupt occurs within a few microseconds. There are no pulses on NRST. I can provide details on the hardware, but this seems to point to a problem with HAL_Init. I will try to modify my production code to eliminate those calls.
2023-12-09 11:27 PM
The trick would be to understand why these precipitate failure, and why interrupts or whatever aren't handled.
2023-12-10 6:38 AM
And now the "external reset" turned into an "external interrupt", which is a totally different thing. If there are no pulses on NRST, then there is no reset either. Most likely what is actually happening here is just an infinite loop and/or hard fault. And you still didn't answer about a watchdog...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.