2025-07-24 5:13 AM
Dear ST Support,
I have two questions regarding the STM32H7S78-DK board.
1. Is it possible to retrieve the original factory application that comes preloaded on the STM32H7S78-DK? I’ve already flashed my own project, but as expected, this process erased the factory-provided firmware.
2. I tried programming the board using a BSP example selected via STM32CubeIDE’s Example Selector. However, the IDE fails to upload the example to the board. A pop-up briefly appears and then disappears, with no further feedback. Even when the board is disconnected, STM32CubeIDE doesn’t display any error or warning that the board is not connected.
Interestingly, when I run my own project, everything works as expected. The board is correctly flashed, and when it’s disconnected, I do receive the expected “ST-LINK not detected” message.
Best regards
Solved! Go to Solution.
2025-11-28 2:19 AM
Hello @Jorge Alves ;
The issue is fixed in STM32CubeIDE 2.0.0 version.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.