2019-09-20 11:51 AM
5. If the device is delivered in an WLCSP143, UFBGA176, LQFP176, TFBGA100 or TFBGA216 package, and the
BYPASS_REG pin is set to VDD (Regulator OFF/internal reset ON mode), then PA0 is used as an internal Reset (active
low)
Can PA0 be used for an interrupt?
2019-09-20 11:53 AM
I'd expect it can be associated with EXTI0, how hard to try?
2019-09-21 2:50 AM
I decided to move this interrupt to another pin.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.