2024-01-25 2:23 PM
Does anyone know where to find a code example for using DCMI on STM32F746G-DISCO? AN5020 says there are 5 examples based on STMCubeMX (section 8.3 p53). But, I can't find any examples for this when I try using STMCubeMX. It doesn't matter which SELECTOR I try.
Nor can I find a code example for this when I use "Import STM32Cube example" in STMCubeIDE.
Thanks,
2024-01-25 10:26 PM
Hello @Hephaestus and welcome to the ST Community :smiling_face_with_smiling_eyes:.
You can implement all 5 projects following the detailed description on the pages 54 to 73 of the AN5020.
PS: capture of JPEG data is implemented using the STM324x9I-EVAL and OV2640 CMOS sensor.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.