STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reuse SWD Pins on STM32F0

I would like to place a user button on PA13 (SWDIO) and PA14 (SWCLK) pins. Reading through the datasheet I find:PA13 (SWDIO) has an alternate function as IR_OUTPA14 (SWCLK) has an alternate function of USART1_TX or USART2_TXBoth pins are listed as FT...

GIoak by Associate
  • 5136 Views
  • 3 replies
  • 0 kudos

STM32F746GDiscovery

5. If the device is delivered in an WLCSP143, UFBGA176, LQFP176, TFBGA100 or TFBGA216 package, and the BYPASS_REG pin is set to VDD (Regulator OFF/internal reset ON mode), then PA0 is used as an internal Reset (active low)Can PA0 be used for an inter...

AD�?b by Senior
  • 1235 Views
  • 2 replies
  • 0 kudos

ST link V3 and reset pin

Hello.I use ST Link V3 to program STM32H753 in SWD mode.I used a programmer in OpenOCD mode.Everything works well. But I control FPGA using ARM.And ARM shares NRST pin with FPGA.So when I program FPM from ARM, I have a problem. When programming FPGA ...

Resolved! How do I disable ST-Link firmware upgrade?

Hello all,The current firmware version for ST-Link does not work properly (I cannot check the memory contents, variables, etc.) Although I could revert to an older version, my IDE (Keil uVision 5.28) opens a pop-up window that suggests me to upgrade ...

ANava by Associate
  • 3161 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.