2021-06-16 2:22 PM
STM32 STLINK Utility has stopped working. I'm sending the setting. What could be the reason?
[Settings]
File=
address=0x08000000
size=0x1000
data_width=4
connection=SWD
SwclkFrequency=15K
freq=8000
Connection_Mode=Normal
DebugInSleepMode=1
Reset_Mode=HWReset
Parallelism=32_Bits
AP_ID=0
RunAfterProge=1
FlashChecksum=0
SkipErase=0
SkipFlashProtection=0
trace.log=1
address1=0x08000000
address2=0x08010000
address3=0x080C0000
[LoopMode]
Device_ID=
MassErase=0
Program=1
Verify=0
OnChipverification=1
OBConfig=0
Run=0
FullChecksum=0
SkipErase=0
SkipProtection=0
OBVal=0000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000
[ExternalLoader]
ElfNumber=1
Elf1=C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\N25Q128A_STM32F746G-DISCO.stldrTarget: Detection Fail
Target Voltage: Detection Fail
Andrzej
Solved! Go to Solution.
2021-06-17 2:18 AM
Hello @Andrzej Dębski
Check connection, USB cables, or maybe you have misplaced jumpers.
Try Connect under reset.
Check if you have problem with reset circuit and check pull BOOT0 low/high.
You can check if you have the same issue with other boards.
Please keep me informed about your progress on this issue.
Thanks
Imen
2021-06-17 2:18 AM
Hello @Andrzej Dębski
Check connection, USB cables, or maybe you have misplaced jumpers.
Try Connect under reset.
Check if you have problem with reset circuit and check pull BOOT0 low/high.
You can check if you have the same issue with other boards.
Please keep me informed about your progress on this issue.
Thanks
Imen
2021-06-17 3:01 AM
The cable is good because I checked on the STM32F3DISCO (it has the same USB).
I am working with FLASH. It happened when the USB cable was disconnected / connected.
Could it be physical damage to the interface? How to check?
Is it possible to program the STM32F746G-DISCO via other USB?
Andrzej
2021-06-17 4:02 AM
Hi Imen!
As I wrote, it seems to me that the chip is damaged. I won't do this anymore unless you have a good idea.
But I remembered that we were contacting about FLASH programming. Based on what to write quickly and efficiently. However, I had laptop crashes (it was old enough) and lost everything. I have to rewrite. I cannot view this correspondence on the current PC. Can you help?
Andrzej
2021-06-18 3:51 AM
I will try to replace U14 and T3. I will write what it gave.
Andrzej
2021-06-24 8:39 AM
I replaced U14 and T3 from the system where the PC-STM communication was. No change.
You wrote "check pull BOOT0 low / high" how to do it?
Andrzej
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.