2024-08-02 1:56 AM - edited 2024-08-02 1:59 AM
I would like to read the level of audio input signal to use like a vu-meter instead of use analog input.
This is my code but I read always 0dB on both channels.
void AUDIO_PLAYER_Init2()
{
/* Allocat mem for Smr */
pSmrPersistentMem = malloc(smr_persistent_mem_size); /* smr_persistent_mem_size 0x188 */
pSmrScratchMem = malloc(smr_scratch_mem_size); /* smr_scratch_mem_size 0xF04 */
if (BSP_AUDIO_IN_Init(INPUT_DEVICE_INPUT_LINE_1, 80, AUDIO_FREQUENCY_48K) != 0)
LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application KO");
else
LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application OK");
}
void Audio_Process2()
{
int32_t error = SMR_ERROR_NONE;
__HAL_RCC_CRC_CLK_ENABLE();
CRC->CR = CRC_CR_RESET;
error = smr_reset(pSmrPersistentMem, pSmrScratchMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err0--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
smr_static_param.sampling_rate = 48000; /* only sampling rate supported */
error = smr_setParam(&smr_static_param, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err1--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
smr_dynamic_param.enable = 1; /* SMR module enabler */
smr_dynamic_param.averaging_time = AUDIO_CFG_SMR_AVGTIME_DEFAULT;
smr_dynamic_param.filter_type = SMR_PREFILTER_AWEIGHTING;
error = smr_setConfig(&smr_dynamic_param, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err2--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
error = smr_getConfig(&smr_dynamic_param, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err4--", LEFT_MODE);
return AUDIO_ERROR_SMR;
}
BufferHandler.nb_bytes_per_Sample = 2; /* 16-bit */
BufferHandler.nb_channels = 2; /* stereo */
BufferHandler.data_ptr = PCM_Data_SMR;
BufferHandler.buffer_size = 32/2; /* just half buffer is process (size per channel) */
BufferHandler.mode = INTERLEAVED;
BufferHandler.data_ptr = &BufferCtl.buff[AUDIO_OUT_BUFFER_SIZE /2];
error = smr_process(pBufferHandler, pBufferHandler, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err5--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
error = smr_getConfig(&smr_dynamic_param, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err6--", LEFT_MODE);
return AUDIO_ERROR_SMR;
}
sprintf((char *)str_pwr, "Left mean power: %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_left*0.25));
BSP_LCD_DisplayStringAt(CHAR(0), LINE(10), (uint8_t *)str_pwr, LEFT_MODE);
sprintf((char *)str_pwr, "Right mean power: %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_right*0.25));
BSP_LCD_DisplayStringAt(CHAR(0), LINE(11), (uint8_t *)str_pwr, LEFT_MODE);
}
2024-08-02 3:10 AM
BSP_AUDIO_IN_Init(INPUT_DEVICE_INPUT_LINE_1, 80, AUDIO_FREQUENCY_48K)
doesn't match the implentation in
hth
KnarfB
2024-08-02 3:33 AM
@aciuf wrote:I would like to read the level of audio input signal
What "audio input signal"? On what board?
@aciuf wrote:but I read always 0dB on both channels.
Have you checked that there is actually any signal present at all?
Is the signal sufficient to read above 0 dB ?
@aciuf wrote:This is my code
So what testing / investigation / debugging have you done on your code to find what's wrong with it?
2024-08-02 4:28 AM - edited 2024-08-02 4:42 AM
I am using a STM32F746-DISCO so INPUT_DEVICE_INPUT_LINE_1 should be the line input.
2024-08-02 4:59 AM - edited 2024-08-02 5:26 AM
Now I see some values but still not good
void AUDIO_PLAYER_Init2()
{
int32_t error = SMR_ERROR_NONE;
pSmrPersistentMem = malloc(smr_persistent_mem_size); /* smr_persistent_mem_size 0x188 */
pSmrScratchMem = malloc(smr_scratch_mem_size); /* smr_scratch_mem_size 0xF04 */
if (BSP_AUDIO_IN_Init(INPUT_DEVICE_INPUT_LINE_1, 100, AUDIO_FREQUENCY_48K) != 0)
//if (BSP_AUDIO_IN_Init(INPUT_DEVICE_DIGITAL_MICROPHONE_2, 80, AUDIO_FREQUENCY_48K) != 0)
LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application KO");
else
LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application OK");
__HAL_RCC_CRC_CLK_ENABLE();
CRC->CR = CRC_CR_RESET;
error = smr_reset(pSmrPersistentMem, pSmrScratchMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_reset--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
smr_static_param.sampling_rate = 48000; /* only sampling rate supported */
error = smr_setParam(&smr_static_param, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_setParam--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
/* SMR dynamic parameters that can be updated here every frame if required */
smr_dynamic_param.enable = 1; /* SMR module enabler */
smr_dynamic_param.averaging_time = AUDIO_CFG_SMR_AVGTIME_DEFAULT;
smr_dynamic_param.filter_type = SMR_PREFILTER_AWEIGHTING;
error = smr_setConfig(&smr_dynamic_param, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_setConfig--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
/* I/O buffers settings */
BufferHandler.nb_bytes_per_Sample = 2; /* 16-bit */
BufferHandler.nb_channels = 2; /* stereo */
BufferHandler.data_ptr = PCM_Data_SMR;
BufferHandler.buffer_size = 32/2; /* just half buffer is process (size per channel) */
BufferHandler.mode = INTERLEAVED;
}
void Audio_Process2()
{
int32_t error = SMR_ERROR_NONE;
uint16_t pbuf[100];
error = smr_process(pBufferHandler, pBufferHandler, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_process--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
error = smr_getConfig(&smr_dynamic_param, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_getConfig--", LEFT_MODE);
return AUDIO_ERROR_SMR;
}
sprintf((char *)str_pwr, "Left mean power: %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_left*0.25));
BSP_LCD_DisplayStringAt(CHAR(0), LINE(10), (uint8_t *)str_pwr, LEFT_MODE);
sprintf((char *)str_pwr, "Right mean power: %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_right*0.25));
BSP_LCD_DisplayStringAt(CHAR(0), LINE(11), (uint8_t *)str_pwr, LEFT_MODE);
}
2024-08-02 5:03 AM
@aciuf wrote:Now I see some values
So what did you change?
@aciuf wrote:but still not good
In what way, "not good"? Give numbers!
Again, are you sure that the input signal you're providing is adequate?
@aciuf wrote:so INPUT_DEVICE_INPUT_LINE_1 should be the line input.
and are you actually feeding it a good, line-level signal?
2024-08-02 5:11 AM - edited 2024-08-02 5:12 AM
Using this last code the dB print without input signal start from 0dB and decrease
2024-08-02 6:49 AM
In the main I call at the begin
AUDIO_PLAYER_Init2
and in a loop
Audio_Process2
2024-08-02 7:14 AM
So what did you change?
I have insert only 2 fuctions in the loop
2024-08-02 10:35 PM
New version
Now I see some correlation from input signal and dB print but still not correct
void *pSmrPersistentMem = NULL;
void *pSmrScratchMem = NULL;
static smr_static_param_t smr_static_param;
static smr_dynamic_param_t smr_dynamic_param;
static buffer_t BufferHandler;
static buffer_t *pBufferHandler = &BufferHandler;
static uint8_t str_pwr[100];
uint16_t PCM_Data_SMR[32]; /* PCM data buffer */
void AUDIO_PLAYER_Init2()
{
int32_t error = SMR_ERROR_NONE;
pSmrPersistentMem = malloc(smr_persistent_mem_size); /* smr_persistent_mem_size 0x188 */
pSmrScratchMem = malloc(smr_scratch_mem_size); /* smr_scratch_mem_size 0xF04 */
if (BSP_AUDIO_IN_Init(INPUT_DEVICE_INPUT_LINE_1, 100, AUDIO_FREQUENCY_48K) != 0)
//if (BSP_AUDIO_IN_Init(INPUT_DEVICE_DIGITAL_MICROPHONE_2, 80, AUDIO_FREQUENCY_48K) != 0)
LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application KO");
else
LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application OK");
__HAL_RCC_CRC_CLK_ENABLE();
CRC->CR = CRC_CR_RESET;
error = smr_reset(pSmrPersistentMem, pSmrScratchMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_reset--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
smr_static_param.sampling_rate = AUDIO_FREQUENCY_48K; /* only sampling rate supported */
error = smr_setParam(&smr_static_param, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_setParam--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
/* SMR dynamic parameters that can be updated here every frame if required */
smr_dynamic_param.enable = 1; /* SMR module enabler */
smr_dynamic_param.averaging_time = 100; //AUDIO_CFG_SMR_AVGTIME_DEFAULT;
smr_dynamic_param.filter_type = SMR_PREFILTER_AWEIGHTING;
error = smr_setConfig(&smr_dynamic_param, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_setConfig--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
/* I/O buffers settings */
BufferHandler.nb_bytes_per_Sample = 2; /* 16-bit */
BufferHandler.nb_channels = 2; /* stereo */
//BufferHandler.data_ptr = PCM_Data_SMR;
BufferHandler.buffer_size = 32/2; /* just half buffer is process (size per channel) */
BufferHandler.mode = INTERLEAVED;
}
void Audio_Process2()
{
int32_t error = SMR_ERROR_NONE;
BSP_AUDIO_IN_Record(&BufferCtl.buff[0], 32/2);
BufferHandler.data_ptr = &BufferCtl.buff[0];
error = smr_process(pBufferHandler, pBufferHandler, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_process--", LEFT_MODE);
return (AUDIO_ERROR_SMR);
}
error = smr_getConfig(&smr_dynamic_param, pSmrPersistentMem);
if (error != SMR_ERROR_NONE)
{
BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_getConfig--", LEFT_MODE);
return AUDIO_ERROR_SMR;
}
sprintf((char *)str_pwr, "Left mean power: %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_left*0.25));
BSP_LCD_DisplayStringAt(10, 100, (uint8_t *)str_pwr, LEFT_MODE);
sprintf((char *)str_pwr, "Right mean power: %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_right*0.25));
BSP_LCD_DisplayStringAt(10, 120, (uint8_t *)str_pwr, LEFT_MODE);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.