STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC trigger

Hello, I want to control the period of ADC conversionsThe code needs to read two adc channels at the same time in a frequency of 10kHz, so, do some maths with this values and output in a DACWhat is the most efficient way to do that?

Nakata by Associate II
  • 1170 Views
  • 1 replies
  • 0 kudos

Is my NUCLEO-F401RE board damaged?

After using the board for a couple of days, the board started giving the following error is Keil-MDK:And the two led's (LD1 & LD3) are always RED as shown below:And the Nucleo USB drivers are installed: I tried also to put the chip into loader mode (...

SamSamuels_0-1722535229229.png SamSamuels_1-1722535323107.png SamSamuels_3-1722535518200.png SamSamuels_4-1722535879278.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.