2024-03-30 7:28 PM - edited 2024-03-30 7:32 PM
After creating my own STM32 PCB, which functions in the same manner as the WeAct BlackPill Development Board (utilizing the STM32F411CEU6), I found myself unable to connect to an external BLE board through UART. I utilized the same pins (Gnd, 3.3V, PA9, PA10) for the pin-out connection, and added nothing else. Is there a reason why I cant read or send anything using the same code from before? Any ideas would be very helpful.
This is the code we are currently using:
while (1) {
/* USER CODE END WHILE /
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1,10);
val = HAL_ADC_GetValue(&hadc1);
char buffer[20] = {'\0'}; //sprintf(out,"%d\r\n",val);
sprintf(buffer,"%d\r\n",val); //CDC_Transmit_FS((uint8_t)buffer,20);
HAL_UART_Transmit(&huart2,(uint8_t )buffer,sizeof(buffer),10);
/ USER CODE BEGIN 3 */ }
2024-03-31 5:03 PM - edited 2024-03-31 5:04 PM
Blinking a LED works?
In debugger, read out and check/post content of UART and relevant GPIO registers.
Observe UART Tx pin using oscilloscope/logic analyzer (LA).
Use a different type of UART connection, e.g. using a UART/USB convertor/cable connected to PC.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.