2019-07-27 8:50 AM
On the STLINKV3 Mini, what is CN3 used for and what are the signals?
Do the two reset pins have a useful user function?
No information on this is available in the current user manual.
Cheers, Hal
2019-07-27 10:08 AM
CN3 is probably the SWD connector used for initial device programming. Have a look at the Nucleo-G47 schematics CN2.
2019-07-27 11:30 AM
Thank You.
No room to say "Reserved" on the Mini.
The Reset pins probably also have a manufacturing only purpose.
Cheers, Hal
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.