2022-07-17 6:37 AM
Hi, I am starting with ST MCU and I would like to start with them on Macbook Pro with M1 chip. I would like to ask if STLINK-V3SET is supported for it. I am a new MacOs user. Thank you very much.
2022-07-18 6:30 AM
Hello @JBaci.1,
Yes, the macOS is supported, please refer to the section 4 of the "STLINK-V3SET debugger/programmer for STM8 and STM32" user manual, UM2448.
I hope my answer helped you. Please mark it as best by clicking on the "Select as Best" button if it fully answered your question, it will help other find that answer faster.
Chahinez.
2022-07-18 7:44 AM
Thank you for your answer and sorry for another one :) So, M1 chip is not problem and drivers for STLINK-V3SET are available? I would like to buy new PRO and I have to be sure that I will be able to program the ST MCUs. Thank you very much for your answer.
2022-07-26 6:09 AM
Hi, please, could you confirm that drivers for M1 are not problem? Thank you very much in advanced.
2022-07-27 2:33 AM
Hi,
I use a MacBook Pro M1 and do operations with STLINK V2.1/V3/V3SET all the time, although I don't use the official ST tools. Tools like OpenOCD or PyOCD should work, and I am the other of a tool called psdb that also works for some MCUs:
We build our firmware on M1 using the arm-none-eabi-gcc package rather than ST tools; I have made a docker container that you can execute from the macOS command line to build repositories and it is available here:
https://github.com/tgree/docker-gcc-arm-none-eabi
If you are planning to use the official ST tools for everything then feel free to disregard the above; it's just an example that it is possible to do serious development on M1.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.