Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I am designing a line-following robot that also avoids various obstacles (two digital infrared (IR) sensors), but I am a bit confused with my schematic since I am a beginner in electronics, and that is why I would like to know if my schematic is corr...
I don't really know where to inform this.Thank.
I am working on a PCB design with a STM32H735IG uC, and I would like to use the integrated SMPS to provide VCORE directly, without the LDO. This corresponds to figure 19.2 of RM0468 (the reference manual). In this configuration the VFBSMPS is connect...
Apologize for IAR specific question, hope someone here can shed some light on my problem. I've tried to ask IAR support, but looks like they have a long weekend or whatever.I have a bootloader at 0x08000000 and main app at 0x08008000.The bootloader ...
// Init L9026 // 00 CHIP_ID, default // 01 CFG0, output high side // W=1,ADD=1,DATA=00111111,P=0,FR=0 HAL_Delay(2); // Set CS lo on L9026 GPIOD->ODR&=(~0x02); // PD1 = 0 data16=0b1000010011111100; SPI_Out_Buffer[0]=SPI_Out_Buffer[2]=SPI_Out_Buffer...
Hi!I got my first programmer like this:https://pl.aliexpress.com/item/32844130786.html?_randl_currency=PLN&_randl_shipto=PL&src=google&src=google&albch=shopping&acnt=708-803-3821&slnk=&plac=&mtctp=&albbt=Google_7_shopping&albagn=888888&isSmbAutoCall=...
Here is the power connection which is in error.
In some situations, CubeIDE (v1.9.0) is not anymore able to handle the communication with the ST-Link probe. Disconnecting the USB cable, restarting CubeIDE, reseting the MCU, nothing allows to make it working again. The only way I found is restardin...
Board: NUCLEO-L552ZE-Q with default setupSW: STM32CubeProgrammerAfter changing RDP from 0 to 1, which was my mistake, I can't connect the board with the program, STM32CubeProgrammer. Whenever I tried to connect, it gave me the error, "Error: ST-LINK ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.