2021-01-16 1:49 PM
I have ST-LINK V2 Programmer and when I connect this with STM32MCU, it shows an error like this I have checked connections, jumper Wire.
Changed the port also. But still, it is showing No STM32 Target Found.
For checking Whether My Programmer is corrupted or not, I have checked ST-LINK with STM8 by connecting to SWIM pinout and it successfully uploads on to my STM8.
So is MY MCU corrupted or damaged, I have an STM32F103C8 Blue chip board.
And have configured its Boot Mode as shown in Pic.
BOOT 0 : 0
Boot 1: opened
Please Help, I am stuck on this for 2 days scratched my head but can't find what the is the issue??
Solved! Go to Solution.
2021-01-21 3:12 PM
Well, I got the solution, I connected my Boot pins like this and then performed the erase chip thing in STM Utility with connecting under reset settings and my chip gets erased successfully and it is working fine now.
But Still, the Problem is coming with STM32CubeIDE.
It is not programming using STM32CubeIDE while successfully getting flashed with STM32CubeProgrammer. Seems there is a problem with my Setting of STM32CubeIDE.
I have raised this query with STM32CubeIDE in separate thread:
2021-07-03 11:40 AM
But there may be no characteristic for deleting an detail from listElements. So I should do is shift different factors and overwrite file to the element that I need to delete?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.