2021-03-22 10:53 AM
I wondering about this in STM32CUBEIDE: Reading 0x20 bytes of memory from addr 0xe00fffd0
MCU: STM32F103RBT6
STM32CUBEIDE log tail (for full log see attachment)
[4.313] handlePacket(): Reading 0x20 bytes of memory from addr 0xe00fffd0
[4.313] write(): <572> Tx: $0000000000000000000000000000000010000000040000000a00000000000000#36
[4.360] read(): <572> Rx: $vKill;a410#33
[4.360] handlePacket(): Hidden/Unsupported v-command 'vKill', see RSP for details
[4.360] write(): <572> Tx: $#00
[4.360] read(): <572> Rx: $k#6b
Stm32CubeProgrammer log:
17:38:27 : ST-LINK SN : 53FF6B065177485738500887
17:38:27 : ST-LINK FW : V2J37S7
17:38:27 : Board : --
17:38:27 : Voltage : 1.90V
17:38:27 : SWD freq : 4000 KHz
17:38:27 : Connect mode: Under Reset
17:38:27 : Reset mode : Hardware reset
17:38:27 : Device ID : 0x410
17:38:27 : Revision ID : Rev X
17:38:29 : UPLOADING OPTION BYTES DATA ...
17:38:29 : Bank : 0x00
17:38:29 : Address : 0x4002201c
17:38:29 : Size : 8 Bytes
17:38:29 : Bank : 0x01
17:38:29 : Address : 0x1ffff800
17:38:29 : Size : 16 Bytes
17:38:29 : UPLOADING ...
17:38:29 : Size : 1024 Bytes
17:38:29 : Address : 0x8000000
17:38:29 : Read progress:
17:38:29 : Data read successfully
17:38:29 : Time elapsed during the read operation is: 00:00:00.006
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.