Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I need to evaluate your MCU of type STM32F407IETDo you have any evalboard with this device?Kind regardsKároly
I wondering about this in STM32CUBEIDE: Reading 0x20 bytes of memory from addr 0xe00fffd0 MCU: STM32F103RBT6STM32CUBEIDE log tail (for full log see attachment)[4.313] handlePacket(): Reading 0x20 bytes of memory from addr 0xe00fffd0 [4.313] write():...
I'm using Stm32f4 nucleo-f412z g for a test fixture kind of setup. After loading the firmware I want to keep the eval board in a box and power it externally with a power brick and usb. But when I do this, it doesn't work with the firmware I uploaded....
32 pins yet there is no target power? How are we suppose to power the target?
Hello i have a jiyi flight controller STM32F407 2 unit faulty and 1 unit is working fine. I use the ST link device to connect the flight controller GND/3.3V/IO/CLK it working on the link msg appear deive memory cannot read, i change the level 1 to 0...
Hi,I am wondering about an apparent discrepancy in documentation of the pin outs for the Nucleo-H743ZI2 board:The "user manual" for the Nucleo-144 boards, on page 7 has in a footnote that H743ZI has been replaced by the H743ZI2. (Link: https://www.st...
I have issue with starting a debug session after upgrading the STLINK-V3SET to version V3J7M2B4S1! I want to go back to firmware V3J5M2B3S1.
Hi everyone,I'm designing my first STM32 design using STM32F103C8and wondering if I can use 2 Ceramic resonators instead of oscillators as shown in my schematic.thanks in advanced!Tommy
Does anyone know what type of Smartcard this is, i get a ICCID and IMSI values that are not consistent with online data
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.