2017-09-16 6:52 AM
How does ST-link V2 affect current measurements of an MCU?
It seems that while connected, it draws quite a lot of current - compared to a low power device.
And how about if the ST-link is disconnected (the USB-cable) from the PC while still connected to the board?
It looks like it still draws current + keeps the core from running.
#st-linkSolved! Go to Solution.
2017-09-16 1:25 PM
Hi.
>>> It looks like it still draws current + keeps the core from running.
Theese effects you described are due to Reset pin of ST-Link connected to NRST pin of your board.
No STLink power , means that NRST pin kept at LO state.
2017-09-16 8:16 AM
A stand-alone ST-LINK, or one on a NUCLEO/DISCO?
The stand-alone takes a VTarget voltage to power buffers/level-converters.
Low-power tends to be about what you're connecting too, and what current pins to the external world sink or source.
Create tests where you don't need an external debugger attached to determine power states and consumption.
2017-09-16 10:46 AM
A proprietary board, and ST-link V2 POD.
And I was wondering especially the effects that an ST-link V2 can cause if left connected to the board (uC via ribbon cable) but not to computer (USB-cable disconnected).
2017-09-16 1:25 PM
Hi.
>>> It looks like it still draws current + keeps the core from running.
Theese effects you described are due to Reset pin of ST-Link connected to NRST pin of your board.
No STLink power , means that NRST pin kept at LO state.
2017-09-16 4:07 PM
That looks like the explanation to what I observed. Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.