Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Posted on September 15, 2017 at 11:53I'm working with a Nucleo F411RE.I've setted JP5 to E5V than I have power up the board from VIN pin. My Chip and application works well, but the STLINK board still working without USB. I can see the Red Led (LD1)...
Posted on January 02, 2017 at 10:40Hi communityI have to write an external loader that is capable of programming a QSPI flash. My hardware design is mostly the same as the STM32F769I-Discovery board. However the pin configuration is different.To und...
Posted on September 05, 2017 at 12:17I'm trying to get a NUCLEO-F411RE to work after removing the ST-LINK, and can't seem to figure out the correct configuration - or maybe it's findings parts.I've been fairly careful, doing things one step at a tim...
Posted on September 04, 2017 at 06:32Greetings People,I have bought STM35F030R8 and was wondering how to connect it with STLink to program the target MCU. I have Discovery F0 board which i can use as STLink programmer. Any guide to connect STM32F030...
Posted on August 30, 2017 at 09:261 https://electronics.stackexchange.com/questions/221895/stm32f407g-disc1-not-working-if-not-connected-to-pc1I have a Discovery board STM32F407G DISC1.I had programmed a Discovery board before with no issues. The o...
Posted on August 19, 2017 at 20:48An ST-Link (from Nucleo-64) don't want to read an STM32F030RCT6 under Windows 10 (64 bit) with a message 'Can not connect to the target'. The most interesting thing is it reads an another same board already programm...
Posted on August 09, 2017 at 16:43I'm trying to recreate my development environment on a new laptop and have run into a strange issue.I've loaded up the latest eclipse, uc plugins, java 8, cross compile toolchain, st-link driver, etc. on a windows 1...
Posted on August 08, 2017 at 10:52Hello,i want to make my own layout with the STM32F103CBT6 as ST-Link, and im not sure, if i can use this Chip as out of the Box ST-Link or if i have to put some firmware on it to use it this way. My Intention is, to...
Posted on July 30, 2017 at 12:42 I'm a little confused about the Stack Size, Thumb and Max Depth shown on the file. Which is generated by the ARM Linker. 1. Where could I found the information what these several words exactly meaning? for ...
Posted on August 04, 2017 at 21:43Hi,We have used J-LINK and J-Flash to program STM32F ARM families for a while and now planning to use ST-LINK and ST-LINK utility instead.We have merged bootloader and application code to make hex file for productio...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.