2018-03-10 3:57 AM
I am trying to program my STM32F103C8T6 from ST link utility but it is showing 'Some Flash Pages are write protected'error while performing full chip erase. I have tried direct programming option in st link utility but it is not programming at all.
https://community.st.com/tags♯/?tags=stlink%20v2
https://community.st.com/tags♯/?tags=stm32f103c8
#stlink-v2 #stm32f103c8Solved! Go to Solution.
2018-03-11 4:22 AM
I have solved this problem using st link utility and removed protection of flash caused by unknown error.
Thank you
2018-03-10 10:06 AM
Are these standard boards, and official ST-LINK? or cheap/boot-leg
Flashing issues like this tend to be issues with communications (connectivity of SWDIO/SWCLK, etc, or USB to the Pod), or at the chip level with power supply issues. The charge pump pulls more current than normal operation, make sure your supply isn't browning out, or signals on NRST either from internal or external POR circuits. The STM32 drives reset by thresholding VDDA.
2018-03-11 4:22 AM
I have solved this problem using st link utility and removed protection of flash caused by unknown error.
Thank you
2018-07-28 4:30 AM
share your solution please
2018-11-14 12:24 PM
Goto:
Target, Option Bytes, Unselect All, Apply.
2021-05-14 10:03 AM
Prasad Dait's and RDean's answer just made me look like a hero.
Removed the write protect bits allowed me to program an unresponsive micro. Good call.
THANKS!
2022-02-28 8:42 AM
hi
that is not working for me "11:38:55 : Some flash pages are read protected!" its a dual core M4 and M7
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.