cancel
Showing results for 
Search instead for 
Did you mean: 

Schematics or information about Nucleo F429ZI?

Cblue_X
Associate II

Hi there!

Im new with ST MCUs and im using a Nucleo F429ZI, i have some documents and one of them is the 'nucleo-f429zi.pdf' but is too short and doesnt have too much information

Im working with user push button connected to PC13 but i want to know if this button has an external pull up/  pull down resistor on the board, and if doesnt i guess i have to set it by software

Where can i found schematics or additional information like this for this board?

Also you would help me if you tell me if PC13 has a pull up/down resistor on the board

Thanks in advance!, sorry for my english, not a native speaker

1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

With the STM32 devboards, you can always find their schematics under "CAD Resources" of their webpage, e.g. for the Nucleo-F429ZI (which btw. is obsolete in favour of Nucleo-F439ZI, which is identical except the 'F439 has enabled the crypto features) here.

JW

View solution in original post

4 REPLIES 4
waclawek.jan
Super User

With the STM32 devboards, you can always find their schematics under "CAD Resources" of their webpage, e.g. for the Nucleo-F429ZI (which btw. is obsolete in favour of Nucleo-F439ZI, which is identical except the 'F439 has enabled the crypto features) here.

JW

Cblue_X
Associate II

Thanks man!, im new to ST so this kind of stuff is not as clear to find for me

What CAD format are these schematics in?

waclawek.jan
Super User

Files in nucleo_144pins_sch.zip as it is in the obsolete 'F429 Nucleo's webfolder?

If you unpack it, it says it in the packed directory's name: NUCLEO-144pins_Altium_Schematics-Layout -  but there's also a standard .pdf in there.

JW