2022-06-13 2:44 AM
I cannot get the VCP function of ST-LINK v3 mini working.
Windows sees the com port and can open it
Connected TX output of UART to pin 14 of ST-LINK 3 mini, but nothing is received on the PC side.
Connected some other serial TTL-USB adapter (set to 3.3V), and it works properly.
However, the serial TTL-USB adapter has a ground connection and ST-LINK's VCP has common ground with other functions.
The debugger function works properly.
Is the TX level of VCP 3.3 or 5 V? Does the VCP function work for anyone?
Thanks,
-- pa
Solved! Go to Solution.
2022-06-13 3:28 AM
Should be 3.3V
Make sure the RX/TX sense is not reversed. Stick a scope on the pins and send stream of data from PC
2022-06-13 3:28 AM
Should be 3.3V
Make sure the RX/TX sense is not reversed. Stick a scope on the pins and send stream of data from PC
2022-06-13 5:41 AM
a) We use the STLINK com port all the time, very convenient with the 14pin MIPI connector.
b) Personally I wouldn't call that VCP as it can be easily confused with STM32 VCP support.
Paul
2022-06-13 3:22 PM
It was a bad soldering. Some software folks are terrible solders (yes it's me). Thanks.
2022-06-13 3:37 PM
I'm an electronics guy, but my soldering skills aren't particularly good, but I have technicians with better skills/technique, better eyesight, and better equipment.. and a lot more practice.
Using high power irons (70-80W), with the right bits, right temperature, and right solder do improve the odds significantly.
I also don't like breadboards, and dupont wires, I much prefer wire-wrap and schmartboard jumper wires, type of thing with good metallic bonds, and can survive a trip around a conference table..
2025-03-01 8:08 AM
This took me a while to find how *** is the RX, TX on ST Link! how on earth they did this?
RX which is receive pin is OUTPUT!, and TX is INPUT! this is most *** think I have ever seen in my life. such a waste of time ...
2025-11-08 9:01 PM
try to connect TX with TX, RX with RX, STLINK V3 MINIE is not the same as other STLINK i have used.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.