cancel
Showing results for 
Search instead for 
Did you mean: 

RealTerm Not Showing Output from Nucleo N657X0Q Board

Aqsa
Associate II

Currently, I am using the Nucleo N657X0Q board, and I am facing an issue with getting my machine learning model output on RealTerm. I am unable to see any output. Does anyone know how to resolve this issue?

2 REPLIES 2
Andrew Neil
Super User

Have you done any basic connectivity tests; eg, confirmed that you can just send "Hello, World" and see it on the terminal?

If not, then do that first!

  • Start with simple direct blocking UART output using  HAL_UART_Transmit():
    https://community.st.com/t5/stm32-mcus/how-to-redirect-the-printf-function-to-a-uart-for-debug-messages/tac-p/733969/highlight/true#M1096
    Don't add any other complications (printf, etc) before you've got this working.
  • Check that you are using the correct UART pins - the ones physically connected to the ST-Link's VCP
    (this is the most common reason for VCP comms not working!)
  • Check that you have the correct COM port selected in your terminal app
  • Check your RealTerm configuration - does it work with any other boards?
    Have you tried other serial terminals?
  • Use an oscilloscope and/or logic analyser to confirm what's actually happening on the wires.

 

Some general tips on Debugging Serial Comms.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
KDJEM.1
ST Employee

Hello @Aqsa ,

 

I advise you to look at this Solved: Re: STM32 N6 UART - STMicroelectronics Community  and check all recommendation shared.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.