2019-09-24 6:35 AM
Hello,
We have developed a custom board having STM32F746NGHx MCU based of the design of the STM32F746G-DISCO board.
We are using ST-Link Utility and ST LinkV3-SET Debugger in JTAG mode to flash.
The board gets flashed and the program is executed after flashing is complete and the display (TFT _ LCD) shows desired output.
But, if the board is reset, the program does not execute and the display shows garbage.
But it executes again only if the STLinkV3-SET Debugger is disconnected and reconnected to the PC.
Please advice on the issue.
Thanks,
Ameya
2019-09-24 7:22 AM
Make sure BOOT0 is pulled LOW so your code runs.
Instrument your code to use a USART so you can understand what's happening internally in the absence of a debugger connection.
Have ErrorHandler() and HardFault_Handler() output actionable data so you can determine what happened if they end up in those routines.
Check timing loops and clocking. Check that external clocks start properly.
2021-02-11 11:30 AM
I had a recent similar condition. Debugger worked but would not boot without debugger. Check the hardware timing of your NRST reset. If the reset time is inadequate you will have a dead brick on power reset but with debugger it gives an adequate reset pulse.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.