2019-04-16 2:02 AM
Hi!
I'm trying to migrate from CoIDE to Atollic and discovered some problems.
It seems that STM32L151CC MCU supports 8MHz maximum speed but I found no option of speed adjusting in Atollic SWD interface. Atollic does not support ST-LINK V1 since v9.1.
Is it possible to program and debug STM32L0, STM32L1 series MCUs via SWD in TrueStudio?
2019-04-16 6:54 AM
Hi M@ks,
There is no possibility to adjust the SWD speed using GUI or command-line with TruesTUDIO / ST-LINK GDB server.
Nevertheless the ST-Link V3 should work with L0 and L1 devices.
Are you unable to program and debug the device?
2019-04-16 7:03 AM
Hi!
Yes, I was unable o program and debug the device. I updated ST-LINK V3 firmware to the latest version. May me it is the reason.
I added STM32Programmer according to this manual manually and set the speed to 4MHz and now it works. http://gotland.atollic.com/resources/applicationnotes/AN1801_cubeprogrammer_in_truestudio.pdf
It seems to be very strange but the programmimg process is successful at the second time only. First programming fails.
Atollic uses STM32Programmer-CLI and it reports an error. Is it possible to resolve my problem without any rain dances with manually adding this programmer?
2019-04-16 7:56 AM
Which version of TS are you using? 9.1.0 or are you now at 9.3.0?
Do you have a Low-power application you are debugging? If the application is in low-power mode while the debugger is trying to connect you may run into problems. If you use external CubeProgrammer tool to erase first, and the TrueSTUDIO/ST-LINK GDB server to program and debug. Does that work consistently?
2019-04-17 1:16 AM
I use TS version 9.3.0. I also tried version 9.2.0 and 9.0.1.
9.0.1 works fine with ST-LINK V1 (STM32VL discovery)
Versions 9.2.0 and 9.3.0 don't work even with fully erased chip.
2019-04-17 1:51 AM
Ok - STM32VL Discovery is the only STM32 board that embeds the ST-LINK v1.
ST-LINK v1 is not supported by STm32CubeProgrammer.
In TS 9.1.0 the ST-LINK GDb server was re-written to use the STM32CubeProgrammer to perform flash operations.
This means that after TS 9.1.0 ST-LINK GDB server can no longer flash program STM32VL-Discovery (since it embeds ST-LINK v1).
So it is unfortunate but expected. Any unanswered questions remaining?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.