2026-04-24 2:06 PM - last edited on 2026-04-25 3:41 AM by Peter BENSCH
Hello,
Started to dwell info embedded development and got my hands on a NUCLEO-H7S3L8 development board. Firstly wanted to analyze the example code that comes with the development board and modify it a bit. But when started to debug, it seems to stop at I and D cache enable functions, and example LED blinking disappeared. Has anyone encountered something similar and could help to fix this problem?
Only change I made to the example code is set-up a PC8 as a PWM to drive a LED switch.
Additionally, tried a mass erase and re-flashing, but still nothing, the problems remains the same as I mentioned.
2026-04-26 6:48 AM
> when started to debug, it seems to stop at I and D cache enable functions,
If you're trying to single-step thru these functions with debugger - just don't. Put a breakpoint outside and run thru these functions at full speed. It is a known issue. Or do you see a different problem?
2026-04-27 6:09 AM
Hello @Domi
Did the original project without your modification work well in debug mode?
Could you precise the name of the example your debugging?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.