2025-04-22 10:40 PM - edited 2025-04-22 10:44 PM
Dear all,
I am trying to make sense of the pin descriptions / pin-mapping of the STM32H7 Nucleo-144 boards, vs. the MCU STM32H723 which it is equiped with.
User manual UM2407 (rev. 4) of the board reads:
However, in the reference manual RM0468 (rev. 3) of the MCU:
Many thanks in advance
Solved! Go to Solution.
2025-04-22 11:33 PM
Hello @LysAn
The UM2407 is the user manual for the NUCLEO-H723ZG, NUCLEO-H743ZI2 and NUCLEO-H753ZI. So, the ADC123_INP10 and ADC123_INP12 does exist on the STM32H743ZIT6 and STM32H753ZIT6 MCUs (available on both NUCLEO-H723ZG and NUCLEO-H743ZI2). That's why they are mentioned on the UM2407. For the ADC12_INP15, it seems to be a typo on the Figure 162 of the RM0468 Rev3 since on the DS13313 Rev 4 we have ADC12_INP15 (that I've escalated to the concerned team for correction on the coming RM0468 versions (under internal ticket number 208346)).
PS: for the alternate functions of the Pins of your board, I suggest to always use the table 7 and 8 of the DS13313.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-22 11:33 PM
Hello @LysAn
The UM2407 is the user manual for the NUCLEO-H723ZG, NUCLEO-H743ZI2 and NUCLEO-H753ZI. So, the ADC123_INP10 and ADC123_INP12 does exist on the STM32H743ZIT6 and STM32H753ZIT6 MCUs (available on both NUCLEO-H723ZG and NUCLEO-H743ZI2). That's why they are mentioned on the UM2407. For the ADC12_INP15, it seems to be a typo on the Figure 162 of the RM0468 Rev3 since on the DS13313 Rev 4 we have ADC12_INP15 (that I've escalated to the concerned team for correction on the coming RM0468 versions (under internal ticket number 208346)).
PS: for the alternate functions of the Pins of your board, I suggest to always use the table 7 and 8 of the DS13313.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.