Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hey everyone, I'm working with the STM32H747I-DISCO board and trying to get it into USB DFU mode to flash firmware using STM32CubeProgrammer. However, the board isn't being detected, and I couldn’t find clear instructions in the documentation about h...
Hello everyone!I've designed a PCB around the STM32H7B0 MCU (I've attached a screenshot of the relevant part of the schematic) for audio signal processing. I wanted to use the maximum clock frequency of 280MHz, but this requires the use of Power Reg...
Can the STM32H757I-EVAL board accept microphone output in formats other than DFSDM or PDM?
Hi,I am working on a project using STM32H757I-EVAL. I wanted to know what the model number of the microphone present in STM32H757I-EVAL. In the user manual, I could just find it as ST-MEMS digital microphones. Also, does it support external microphon...
Hi ,I'm working on a code to collect data from a load cell wit HX711 cip. I'm using STM32CubeIDE.I configured GPIO pin 6 as Clock output for the HX711 but when calling HAL_GPIO_WritePin the output pin PA6 does not change.The hardware configuration is...
I am currently using the STM32F103C8 board, in this, I connect the OPTOCOUPLER input to the PA6 PIN of stm32 which is the PWM pin, and at the output side I connect the optocoupler's output to the driver's 10v + pin and optocoupler's output with 10v ...
Hello, I made a custom board using the STM32C031K4T6. I have tried several times now to connect to the chip using STM32 Cube IDE and the STM32 Programmer, both didn't work. The ST-Link gets recognized. I have tried different combinations regarding th...
Custom board will not run without debugger. With debugger removed and cycling power I have manually touch NRST to ground to get it to run.The NRST is only connected to SWD pin, but when debugger is removed it is not connected. Theis is no ST-LINK o...
Hi,I am looking for an LCD Touch display for B-U585I-IOT02A Discovery kit but I could not find any. Is this possible to connect a local Touch LCD screen to the B-U585I-IOT02A Discovery kit? It looks like the STM32U585AI MCU does not contain any displ...
Hi, Could you list NUCLEO-H753ZI board's ADC1/2 ADC3 channel Index with GPI/O Pin assignment table with the connector name / pin index on the board, using channel number as the index It is very difficult to configure CUBEMAX-ADC without this Ta...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.