2020-09-29 9:54 AM
I have recently purchased a NUCLEO-L031K6 dev board and when connecting it via USB ST-Link won't get recognized. I have 2 other st-link which work like a charm, so drivers are there (STM Discovery F0 and ST-Link V2). Any help? Is there any boot sequence to follow for the ST-Link on the NUCLEO-L031K6 to be recognized ?
Solved! Go to Solution.
2020-09-29 10:11 AM
Nothing special about the board. Make sure you're not using a charging cable (without data lines connected).
2020-09-29 10:09 AM
Hello @picatostas ,
Have you tried using STM32CubeProg tool ?
Imen
2020-09-29 10:11 AM
Nothing special about the board. Make sure you're not using a charging cable (without data lines connected).
2020-09-29 10:34 AM
Yes I tried first with that !
2020-09-29 10:34 AM
Good point, kind of shameful if my first post here is such a noob mistake :E
2020-09-29 10:38 AM
it was that indeed. Thanks! Happy Coding!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.