Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
we are using two micro controller one is nucleo L4R5ZI Board with STlink on board can be used as independent programmer and 2nd is ARM9 . we want to use this ST link programmer to program a ARM9 processor. is it possible? is STLink support older ve...
I have recently purchased a NUCLEO-L031K6 dev board and when connecting it via USB ST-Link won't get recognized. I have 2 other st-link which work like a charm, so drivers are there (STM Discovery F0 and ST-Link V2). Any help? Is there any boot seque...
I'm looking to use the Arduino header on the STM32H7B3i-DK, however I am finding an inconsistency between what is defined in the Schematic and what is listed in the Users Manual.Example: For header C10 Pins 1 and 2: The schematic shows these mapp...
I have just recieved this circuit board and im trying to program it with an ST-LINK V2 however i keep getting the error "no stm32 target found" when trying to connect to it through SWD. Could someone help me?
Hi,I am using STM32 controller (STM32L475VC) for our project. I am getting error as "NO TARGET FOUND" whenI am trying to debug through ST-Link V2 orTrying to access the controller for Erase/Program with STM32CubeProgrammerI have done following steps ...
It is from UM1472 User manual ,,, file:///C:/Users/Yeni/Desktop/stm32F407/dm00039084-discovery-kit-with-stm32f407vg-mcu-stmicroelectronics.pdf ,,, I am trying to use UART with Tera Term,As can see , The ST-LINK/V2-A supports a virtual COM port (VCP) ...
We're evaluating STM32 controllers in our product. We have shortlisted the following 3 MUCs from STM32H7, STM32F7 & STM32F4 which has same IC package - UFBGA176+25 (10 x 10 mm).Any one MCU will be used in the design. Our intent is to change MCU based...
Hi,Can ST-Link be used to program both M0 and M4 cores? Also if the controller in STLink is replaced with STM32WB55RG can the driver for STLink be customized or does it require a new driver development? Is the driver open source? If yes, on what form...
Hi, Thank you for reading this question.I am using STM32F429 for hardware-in-the-loop (HIL) simulation. The emulator is OPAL-RT. However, I did not find any relevant information about HIL in ST community. Can anyone share some information or where ca...
Good Morning,I am currently using a Nucleo -board stm32g474re, but I am unable to configure eclipse to connect to the Nucleo using the ST-Link v3.Is it possible to configure eclipse to debug using the ST-Link v3 of the Nucleo board?In the past with N...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.