cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7B3i-DK - Inconsistency between Schematic and Users Manual for Arduino headers

JMors.1
Associate III

I'm looking to use the Arduino header on the STM32H7B3i-DK, however I am finding an inconsistency between what is defined in the Schematic and what is listed in the Users Manual.

Example:

For header C10 Pins 1 and 2:

The schematic shows these mapped to MCU Pin PF10 and PI7 respectfully.

The User's Manual shows this mapped to MCU Pin PD1, PI2 respectfully

For header C11 Pin 1:

The schematic shows this mapped to PH14

The User's Manual shows this mapped to PB11

Header CN20, Pins 1, 3, and 4 do not match between the Schematic and User's Manual.

Reference:

User Manual: https://www.st.com/resource/en/user_manual/dm00610478-discovery-kit-with-stm32h7b3li-mcu-stmicroelectronics.pdf

Schematic:: https://www.st.com/resource/en/schematic_pack/mb1332-h7b3i-b02_schematic.pdf

Is there a way to verify which is the correct one?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Yeah, I had seen that, however I have a B02 version board so I was just matching the schematic to the board.

I do think the User's Manual is more likely wrong.

View solution in original post

5 REPLIES 5
TDK
Super User

> Is there a way to verify which is the correct one?

Two options:

  • Probe for continuity between the pin and the output. Easy if you have fine enough probes.
  • Set the pin as GPIO and toggle it. Measure the output with a multimeter/scope/logic analyzer.

If you feel a post has answered your question, please click "Accept as Solution".
JMors.1
Associate III

I suppose I had to clarify my question.

Would it be possible that someone from ST could clarify which is correct; the User;s Manual or the Schematic, or just correct the documentation?

Andreas Bolsch
Lead II

There's already a newer schematic https://www.st.com/resource/en/schematic_pack/mb1332-h7b3i-c01_schematic.pdf

But there seems to be no difference relative to B02 regarding the Arduino connectors.

Yeah, I had seen that, however I have a B02 version board so I was just matching the schematic to the board.

I do think the User's Manual is more likely wrong.

Mike_ST
ST Employee

Thank you for reporting.

The schematics (B02 or C01) are correct.

The User's Manual will be updated.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.