2023-10-15 1:12 AM - edited 2023-10-15 1:20 AM
I am only used to writing C scripts on RPi, so I'd like to apologize in advance if I left something vague.
I was looking to use ISPU for LSM6DSO16IS and the website recommended NUCLEO-F401RE as one of the options for developing the project. I am thinking of getting started with NUCLEO-F401RE but I have a question before I buy one.
It says in the link (https://www.st.com/content/st_com/en/campaigns/ispu-ai-in-sensors.html) that NUCLEO-F401RE is one of the "STM32 Open Development Environment". Does this mean that I can write a C script for LSM6DSO16IS that fully utilizes ISPU and the sensor library using STM32Cube with NUCLEO-F401RE and use the C script in other MCU's, such as Raspberry Pi boards?
2023-10-15 2:32 AM
You'd probably want to review if the libraries are pre-built and for what platforms, and if source for those libraries is provided or not.
2023-10-15 6:14 AM
If you want to use the sensor with both the STM32 and Raspberry Pi, you may need to write separate code for each platform.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.