STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 CAN bus 2.0B

Hello, I'm working on a project where I need to read the CAN bus messages that are coming from an ECU. I'm using the STM3210E-EVAL that has the STM32f103ZGT6. I'm reading the CAN bus messages with the following function: void HAL_CAN_RxFifo0MsgPendin...

Smdeint by Associate III
  • 2515 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 and Platformio

I have been developing a program for the Nucleo-32 (STM32L412KBU6) board in Visual Studio Code's Platformio, and I have run into an interesting problem. I am able to build my project with no errors and upload it successfully. However, whenever the co...

caden013 by Associate II
  • 3811 Views
  • 3 replies
  • 0 kudos

pwm complementary Mode not getting Invertered output ie HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1);

I am using STM32f103 Controller ,In that i am trying to make complementary PWM output by using Timer 1TIM1 with PWM Generation CH1 CH1N ,But only gets the wave from this HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1); function not getting other inverted si...

SD card interfacing with stm32l432kc

Hi, I am using STM32l432kc board with sd card module. I have 16gb class 10 sd card.  I have used cubemx ide for coding and configuration purpose. I am using @https://microcontrollerslab.com/microsd-card-module-stm32-blue-pill-stm32cubeide/ and also s...

kushal by Associate
  • 1892 Views
  • 1 replies
  • 0 kudos

NUCLEO-F401RE question

I am only used to writing C scripts on RPi, so I'd like to apologize in advance if I left something vague.I was looking to use ISPU for LSM6DSO16IS and the website recommended NUCLEO-F401RE as one of the options for developing the project. I am think...

el659 by Associate III
  • 1788 Views
  • 2 replies
  • 0 kudos

Problems starting debug of F439ZI

Hi, I sometimes get this error when starting a Debug on an F439ZIError in final launch sequence: Failed to start GDB serverFailed to start GDB serverError in initializing ST-LINK device.Reason: (5) Unknown MCU found on target. Unplugging and repluggi...

alanb by Associate II
  • 2120 Views
  • 3 replies
  • 0 kudos

Resolved! UART Communication Issue

Hi, I am using G474RE nucleo board and I want to communicate between the UARTs available on the board (UART2,UART1 and UART3). Message is not transmitting complete in to UART1 from UART2 and same with UART3 from UART1 

VGani.1 by Associate III
  • 2429 Views
  • 3 replies
  • 0 kudos

Reference schematic - STM32F103VET6 MCU

Dear team,We are currently in the process of designing a custom board centered around the STM32F103VET6 MCU. Unfortunately, we have been unable to locate a reference schematic that features this specific MCU. We kindly request the following informati...

sivam by Associate II
  • 3703 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.