2025-03-14 3:51 PM
Hello,
I previously used ST-LINK V2, which worked fine, but due to its lack of a Virtual COM Port (VCP), I recently purchased a NUCLEO-64 (STM32F030R8 EVAL BRD) to program my own PCB using its ST-LINK.
The Nucleo board itself works fine, but when I try to use its ST-LINK to program my own PCB (using STM32G030F6P6TR), I encounter issues despite following the manual:
I have been troubleshooting this for days but found very few resources on using a Nucleo board's ST-LINK for external programming.
As mentioned, the Nucleo board itself works fine, and my PCB works with ST-LINK V2, but not with this Nucleo ST-LINK.
Do you have any insights on why this might be happening?
2025-03-14 5:01 PM - edited 2025-03-14 5:02 PM
> Without external power: STM32CubeProgrammer does not connect.
This is expected as CN4 does not provide power.
> With external power: CubeProgrammer connects but disconnects after ~10 seconds, then crashes.
Any error messages? Does lowering the speed help? Updated ST-Link firmware?
Ground loops could always cause an issue. Can you power it from the nucleo board and see if that changes things?
2025-03-15 2:22 PM
Hello,
Thank you for your comment.
Yeah, I tried all kinds of things, including updating the firmware...
Strangely, I connected the Nucleo board to another STM32 dev board, and it worked. Then, I reconnected the Nucleo back to my custom PCB, and it worked halfway—it stopped crashing but still couldn't be programmed. After that, I connected my second custom PCB (which is exactly the same as the original one I was working on), and it worked. Then, when I reconnected my original PCB, it started working as well...
I really don’t know what’s happening, but now I can program. However, USART still doesn’t work. Maybe I need to snap the ST-Link part to use USART on my custom PCB, perhaps...
2025-03-15 2:50 PM
Probably a bad solder joint somewhere or other manufacturing issue. Could also be a design issue.
2025-03-16 1:19 AM
Dear @Manowi25 ,
Can you share your target MCU part and good resolution photo soldered on the PCB ?
Ciao
STOne-32
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.