2024-03-12 4:00 AM
We use a an STM32L4R9-DISCO board to start SW development on a project.
We run own OS on the board and integrating the HAL/BSP modules for the board (e.g. STM32CubeL4\Drivers\BSP\STM32L4R9I-Discovery\stm32l4r9i_discovery_io) is not feasible for us.
I have basic I2C running (ack from the MFX) but no reaction to any commands, using the registers defined in mfxstm32l152.h
I therefore need basic documentation of the MFX_V3 I2C communication for setting up port directions, getting and setting ports.
rgds Tage
2024-03-12 4:10 AM
Okay setting MFXSTM32L152_GPIO_EN in MFXSTM32L152_REG_ADR_SYS_CTRL helped.
I would still like to be pointed to some documentation on the MFX_V3.
2024-03-12 7:44 AM
Hi @tkorsdal
The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.
Regards,
Billy
2026-01-17 1:33 AM
Hello,
I am in the exact same situation as the original poster.
I am currently working with the STM32H757I-EVAL board and I need to interface with the onboard MFX (STM32L152, MFX_V3) for IO expansion and power monitoring.
I have been searching for the official documentation and the latest source code/drivers specifically for MFX_V3, but I haven't been able to find a comprehensive guide. Could you please provide the datasheet (or register map) and the official driver source code?
Any help would be greatly appreciated.
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.