2024-09-26 10:55 AM
I have an STM32H7B31-EVAL board setup with TouchGFX. I am able to compile and load a project using STM32CubeIDE. I would like to be able to do the same from the command line. I found this document that gives a very basic outline of the STM32_Programmer_CLI program. I am able to load the MCU portion of the program this way, but I can't find any documentation on how to use it to load the external flash. In CubeIDE, I have an external loader selected (MX25LM51245G_STM32H7B3I-EVAL-REVB.stldr). I'm not sure how to use this setup from the command line. Links to documentation or existing solutions would be appreciated.
Solved! Go to Solution.
2024-09-26 3:35 PM - edited 2024-09-26 3:37 PM
Takes the form of the following to read the content out, --download variant to program, will find an example
STM32_Programmer_CLI -c port=swd --vb 3 --log test_5m6.log --extload C:\STM32Cube\STM32CubeProgrammer_v2.10.0\bin\ExternalLoader\CLIVEONE-W25Q512_STM32L4XX-PB10-PA2-PE12-PB0-PE14-PE15.stldr --upload 0x90000000 0x559298 test_5m6.binSee attached command line help screen
2024-09-26 3:35 PM - edited 2024-09-26 3:37 PM
Takes the form of the following to read the content out, --download variant to program, will find an example
STM32_Programmer_CLI -c port=swd --vb 3 --log test_5m6.log --extload C:\STM32Cube\STM32CubeProgrammer_v2.10.0\bin\ExternalLoader\CLIVEONE-W25Q512_STM32L4XX-PB10-PA2-PE12-PB0-PE14-PE15.stldr --upload 0x90000000 0x559298 test_5m6.binSee attached command line help screen
2024-10-02 7:55 AM
For my specific setup, I did the following:
./STM32_Programmer_CLI -c port=SWD freq=8000 reset=HWrst \
--extload ./ExternalLoader/MX25LM51245G_STM32H7B3I-EVAL-REVB.stldr \
-w /path/to/file.hex
Note that the STM32_Programmer_CLI program needs to be run from the its directory (at least in Linux). For example, I have the utility in /opt/stm32/bin. Not being in this directory will result in error messages like "Unable to list supported devices".
Thanks for the assistance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.