cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-C031C6 duplicate net name on Morpho connector

Karl Yamashita
Principal

 

I believe that the net name on CN7-4 should be PD3. 

Nucleo-C031_doubleNetname.jpg

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Karl Yamashita @Andrew Neil 

After checking with our HW team, I can confirm that both connectors CN7-3 and CN7-4 are mapped to the same pin of the MCU (PD2).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
STTwo-32
ST Employee

Hello @Karl Yamashita 

Thank you for this contribution. I'm checking internally and i will be back to you ASAP.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Fig 7 in UM2953 is the same:

AndrewNeil_1-1727801087393.png

 

PS:

PD3 is on CN10.1 both in schematic and in UM2953 Fig 7

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
STTwo-32
ST Employee

Hello @Karl Yamashita @Andrew Neil 

After checking with our HW team, I can confirm that both connectors CN7-3 and CN7-4 are mapped to the same pin of the MCU (PD2).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Karl Yamashita
Principal

As @Andrew Neil, PD3 is on CN10, which i missed.

Though it doesn't make sense to have PD3 by itself when it could have been grouped with the other 3 PDx pins. Unless there is a reason to have PD3 on CN10?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.