2025-04-18 3:54 AM - last edited on 2025-04-22 2:31 AM by Amel NASRI
Hello,
I am using STM32L0 microcontroller in my device. I put my device in deep sleep and wakeup using the same button by sorting SYS_WAKEUP2 pin and nearby PC14 is used as an Input pin (pulled-up).
The issue is when I disconnect & reconnect USB power to the my device, it does not start at all. Below I have attached my code and circuit.
SYS_WAKEUP2 pin:
BOOT0 & NRST connection:
System wakeup pin and connection with button:
Here is my code to go into deep sleep which used for "long press ON":
if(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_14)== GPIO_PIN_SET)
{
// Start the equipment
HAL_GPIO_WritePin(PERIPHERAL_EN_GPIO_Port, PERIPHERAL_EN_Pin, SET);
HAL_Delay(20);
lcd_init();
ClearLCD();
StartTick = HAL_GetTick();
char strr[20];
while(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_14)== GPIO_PIN_SET)
{
FinalTick = HAL_GetTick();
TickCount = FinalTick-StartTick;
if((TickCount % 1000) == 0)
{
init_columnset(3, 20);
sprintf(strr,"Wakeup in %u ",PowerOn);
GLCD_Bold_String(3, &strr);
PowerOn++;
}
if(PowerOn>=5) break;
} // end of while loop
if(PowerOn<5)
{
init_columnset(3, 15);
GLCD_Bold_String(3, "Shutting Down... ");
HAL_Delay(1000);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_SuspendTick();
HAL_PWR_EnterSTANDBYMode();
}
} // end of If condition
else
{
//shutdown
init_columnset(3, 15);
GLCD_Bold_String(3, "Shutting Down... ");
HAL_Delay(1000);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_SuspendTick();
HAL_PWR_EnterSTANDBYMode();
}
Please help me to solve this issue, Thank you so much for the help.
2025-04-22 3:43 AM - edited 2025-04-22 3:43 AM
Hello @JeetS,
As far as I can see; BOOT0 is pulled down, NRST is pulled up, seems correct!
Are you sure of the stability of the power supply?
And what do you exactly mean by "it does not start at all", are you having some code to blink an LED or send a msg over UART for example and it's not working as expected? or the your device is not powered at all?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.