2018-02-06 4:47 AM
Hello,
I'm starting a new project with the STM32F746 and I would like to know if I can connect the STLINK/V2 �NRST� output pin (pin 15) directly to a switch, with one of the terminals grounded or directly to a microprocessor supervisory circuit, like the ADM6713.
What is the minimum resistance value that I can put like pull-up, in the NRST signal originated from STLINK/V2?
Thanks!
#stm32f7 #stlinkv2(v2) #jtag2018-02-06 5:01 AM
If you look at the nucleo/dico boards schematics, the black buttom shorts NRST to ground.
The Stlink NRST output however also shorts NRST from the target to ground when the stlink is unpowered. It is a pity that a non 5-volt tolerant pin has been choosen...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.