2020-10-20 1:53 PM
Hello All,
I have the following setup:
These are the problems I am seeing:
The voltages on the other configured inputs and outputs are all fine except for these two. I have tried using internal pull-up resistors instead of external ones, but the results are the same. I have also tried using older L4 firmware packages besides v1.16.0 but again, it made no difference. Are there any known issues with pins PB11 and PB9 on this particular MCU? Any suggestions?
2020-10-20 2:38 PM
Have you got a pull down on the BOOT0 pin (PH3 - pin 44)? Maybe the bootloader is running.
2020-10-20 3:57 PM
> When pin is grounded, current shoots up to 230mA.
There aren't any pin settings that are going to let you pull 230mA out of PB11. Look for a hardware issue, maybe a short somewhere else. Measure impedance from PB9/PB11 to ground and to 3.3V. It's also possible these are damaged. 1.2V is roughly the internal operating voltage. Not sure what failure mechanism could cause that, but maybe there is one.
In any case, even if they are configured as output, 1.2V is not a valid digital output. It'd be 3.3V or GND.
See what part heats up when you ground PB9.
2020-10-21 5:18 AM
Pin 44 (PH3-BOOT0) is not configured as anything and there is no resistor connected to it (floating). There is some UART handling logic running in the main loop, but it is mostly idle.
2020-10-21 5:16 PM
2020-10-22 4:46 AM
Thanks for the link. I realized after I posted my first reply that I had made an error - the BOOT0 pin actually WAS tied to GND via a 4.7K resistor. I did try removing it to see the effect on the pins in question, but found that the MCU does not restart properly as described in your link.
2020-10-28 11:15 AM
Just got off the phone with ST technical support staff and was told that the particular MCU I am using (STM32L4Q5CGT6P) with the letter 'P' at the end of the part number has two switch mode power supply output pins on exactly the two pins I am having issues with - pins 22 and 46. This explains why my power supply current reading shot up when I grounded pin 22, and it also explains why I could not get SDA_1 on pin 46 to budge no matter what I tried. Neither the datasheet nor CubeMX makes any reference to these two special pins. In fact, CubeMX does not even let you choose this particular MCU with the 'P' variant. ST mentioned that they will raise an internal ticket to have the datasheet and CubeMX corrected to show the 'P' variant of MCU. Hopefully this will save someone out there a lot of time and frustration.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.