STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLINK-V3 CLI erasing eeprom

Hi,I am using the below on the command line (STM32_Programmer_CLI) to erase full IC.-c port=SWD mode=UR Freq=8000 -e all'But it does not erase eeprom, is there another command to erase eeprom?

JFOLE.1 by Associate II
  • 1673 Views
  • 1 replies
  • 0 kudos

Nucleo-F767ZI No ST-Link detected.

So I have a Nucleo-F767ZI development board and I wanted to try out some applications on it but unfortunately once I try opening the debugger it gives me a "no st-link detected" error message. I have a Mac running running the latest version of macOS....

Is there a possibility to read program counter via ST-Link or J-Link without causing a reset on STM32F103 devices with RDP active?

On a serial product after a firmware update, there are some sporadic cases, where we get a hang up situation. It would be very helpful to know where exactly the program is stuck. According to ES0346 Rev. 6 chapter 2.8 it is possible to access progra...

stst9185 by Associate III
  • 7151 Views
  • 13 replies
  • 0 kudos

Incorrect voltage on input pin of STM32L4Q5CG when pulled-up to supply voltage via external resistor

Hello All,I have the following setup:Stand-alone STM32L4Q5CG on 48-pin breakout board with coupling caps installedPB11 tied to 3.3V via external 4.7K pull-up resistorPB9 tied to 3.3V via external 4.7K pull-up resistorSTM32CubeMx rev. 6.0.1 Firmware p...

ebce3 by Associate II
  • 2688 Views
  • 6 replies
  • 0 kudos

Resolved! Read and write using ST-Link V2

Hi everyone,I do have 2 PCB boards based on STM32F030F4P6 MCU, the two PCBs have the same hardware and connection with other components, I read the first MCU's code using ST-LInk V2 -using SWD- and saved the .hex file to my PC then I wanted to re-pro...

AKh.2 by Associate II
  • 12233 Views
  • 12 replies
  • 0 kudos

LDO for STM32L433?

Hello, I would like to know what LDO regulator you recommend to use in my development, it uses a 7.2V Lithium battery pack. The application uses 5 GPIO's (4 output, 1 input), 1 I2C, 2 USART, 1 LPUART.

AStol.2 by Associate II
  • 2148 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.