2021-01-07 2:29 PM
I'm trying to flash/debug a B-L072Z-LRWAN Discovery kit from Ubuntu 20.04 using openocd, but its failing to connect:
openocd -f interface/stlink-v2-1.cfg -f target/stm32l0.cfg
Info : auto-selecting first available session transport "hla_swd". To override use 'transport select <transport>'.
adapter speed: 300 kHz
adapter_nsrst_delay: 100
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
none separate
Info : Unable to match requested speed 300 kHz, using 240 kHz
Info : Unable to match requested speed 300 kHz, using 240 kHz
Info : clock speed 240 kHz
Info : STLINK v2 JTAG v37 API v2 SWIM v26 VID 0x0483 PID 0x374B
Info : using stlink api v2
Info : Target voltage: 3.248915
Error: init mode failed (unable to connect to the target)
What configuration do I need to connect to the embedded stlink-v2-1?
2021-01-07 2:33 PM
Is there a "connect under reset" type option? Some of the firmware goes into a sleep mode and will turn off the logic you're trying to work with.
Should be able to sustain a faster clock (couple of MHz as I recall, but not 24 MHz)
2021-01-07 2:46 PM
OpenOCD has nothing I can see that seems applicable, its all rather JTAG-oriented.
2021-01-07 2:56 PM
Got it, thanks. The stm32l0.cfg config file needs to use
reset_config srst_only srst_nogate connect_assert_srst
2021-01-10 2:42 PM
However, when I try to connect to openocd using gdb, I encounter a further problem:
$ openocd -f interface/stlink-v2-1.cfg -f target/stm32l072.cfg reset init
Open On-Chip Debugger 0.10.0
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "hla_swd". To override use 'transport select <transport>'.
adapter speed: 240 kHz
adapter_nsrst_delay: 100
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : clock speed 240 kHz
Info : STLINK v2 JTAG v37 API v2 SWIM v26 VID 0x0483 PID 0x374B
Info : using stlink api v2
Info : Target voltage: 3.262228
Info : stm32l0.cpu: hardware has 4 breakpoints, 2 watchpoints
Info : accepting 'gdb' connection on tcp/3333
Warn : Cannot identify target as a STM32L family.
Error: auto_probe failed
Error: Connect failed. Consider setting up a gdb-attach event for the target to prepare target for GDB connect, or use 'gdb_memory_map disable'.
Error: attempted 'gdb' connection rejected
It knows its an stm32l0 CPU, but also it doesn't... what can I try?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.