2026-04-20 11:10 PM - last edited on 2026-04-22 3:19 AM by KDJEM.1
It looks like I have the 32F469IDISCOVERY board that looks to be powered ok via USB connector CN13, however the board doesn't appear to have demo software preloaded. COM LED LD6 flashes red.
I note on the ST website that there is the 32F469IDISCOVERY compiled demo binary, which I have downloaded.
The Readme says: The QSPI external flash loader is not integrated with supported toolchains, it ís only supported with
STM32 ST-Link Utility V3.7 or later.
But the ST website says that the ST-Link Utility is NRND and to use STM32CubeProg instead. I've tried the latest version of STM32CubeProg and it can't connect to the board via USB:
Error: Establishing connection with device failed.
What is the best way of programming the board with this file please?
Kind regards,
Al
Solved! Go to Solution.
2026-04-22 1:50 AM
2026-04-22 2:00 AM
@alw wrote:I was just looking for clarity on how to load the demo binary
As already noted, do that via the built-in ST-Link, on CN1.
The User Manual tells you that the board is designed to be powered this way.
The original demo won't require anything other than the board itself.
2026-04-22 2:29 AM
> The original demo won't require anything other than the board itself.
And not even to flash this demo.
All discovery boards I have (F303 and F407) came pre-loaded with the respective demos.
2026-04-22 2:34 AM
@Ozone wrote:
All discovery boards I have (F303 and F407) came pre-loaded with the respective demos.
Indeed.
@alw if your board is new, and it doesn't have the demo loaded, you should contact the supplier to get it replaced.
2026-04-23 1:29 AM
I just tried powering via VIN on CN6, with the same result.
So I am guessing that it wasn't programmed with the demo.
There's a small test label on the side of CN7 which maybe tells us all we need to know...
T1: Tick T2: Tick T3: Tick T4: Tick QA:
So no Quality Assurance check. I will take the issue up with the ST distributor.
Thanks for all your help.
Kind regards,
Al
2026-04-23 1:46 AM
Hello ,
Please confirm that: are you able to connect to the board over CN1 (STLINK-USB)? forget about VIN, and other power supply sources for now..
We need to avoid unnecessary ping pongs.
2026-04-23 1:55 AM - edited 2026-04-23 1:57 AM
Hi @mƎALLEm
It doesn't work with powering via CN1 (ST-LINK USB) either via a USB power adapter, or connected to my Mac as it doesn't connect to STM32CubeProg regardless of whether I select UART, ST-LINK, J-Link/Flasher or USB.
Neither does anything appear to be functioning if I try to do an ST-LINK firmware upgrade via STM32CubeProg.
Kind regards,
Al
2026-04-23 1:59 AM
OK.
So let's summarize:
1- You have a brand new 32F469IDISCOVERY board.
2- You are not able to connect to the MCU with STM32CubeProgrammer over CN1 (ST-LINK USB)
Could you confirm the two points? Am I correct?
2026-04-23 2:52 AM
Both are correct, I received the board some months back but it's the first time I've tried using it.
Kind regards,
Al
2026-04-23 2:56 AM
Have you done the basic connectivity checks to see if your Host system can even see the ST-Link at all ?
This is written in Windows terms, but Mac must be similar...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.