2024-07-11 11:04 PM
I am fairly new to the STM32 world. i got an "original" old board lying around in the office, which am using. i cannot directly "load" my code into it it shows error to me that my st-link is not upgraded, after opening the ST-LINK upgrade, it does detect the version etc but when i click on "Yes>>>>" it shows an error. i have been working with uploading the hex file through stm32 ST-LINK utility and i am able to upload and run my code, any possible solutions or atleast, anyone has any idea about what the problem could be?
2024-07-11 11:34 PM
I am getting this kind of error. Utility can see my blue pill but cant debug in stm32cubeide interesting and the problem with that might be stlink you use.
2024-07-12 12:09 AM
its an stm32f429 discovery board, it is supposed to have ST-LINK embedded on the board itself. so i dont think how that is the problem, or, you are saying that the ST-LINK hardware on my board is troubled or smth
2024-07-12 12:36 AM
most likely the st-link but wondering if this is your first time using that stlink? And you know that's kind of upgrade after all so gotta check tha port numbers that are used.
2024-07-12 12:53 AM
dont think so, because when i first got the board and plugged it in, it was already running a code displaying internal temperature on the LCD
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.