2019-09-23 12:20 AM
Hi,
I am working on STM32F042K6T6(LQF-32) ARM microcontroller with STM32CubeMX and Keil software, according to the datasheet boot0 pin is available in pin-31 but when I open the same controller in STM32CubeMX I am neither finding any such pin nor its function like BOOT0
So should I include 10k ohm resistor at pin-31 and ground it irrespective of its availability?
Can anyone help me out here?
Regards
Shivakumar
2019-09-23 12:25 AM
Yes, you should have a pull down to ensure consistent start up performance.
2019-09-23 12:43 AM - edited 2023-11-20 9:29 AM
Thank you Clive!
Even though there is no BOOT0 function available in the pin-31(PB8) as attached in the image here, I should directly connect a pull down right?
Otherwise(if I do not use pull down) is there any chances of reading garbage data from stored flash data everytime when I restart the controller?
Regards
Shivakumar
2019-09-23 12:59 AM
> Otherwise(if I do not use pull down) is there any chances of reading garbage data from stored flash data everytime when I restart the controller?
A floating BOOT pin will make your board startup into system mode (ROM bootloader) or other modes seemingly at random.
> Even though there is no BOOT0 function available in the pin-31(PB8) as attached in the image here, I should directly connect a pull down right?
BOOT0 is not "selectable functionality" - it is the pin's functionality at startup (POR), before you application. Check the datasheet.
2019-09-23 1:16 AM
Thank you Ozone!!
I got your point but i'm getting confused after referring the datasheet because, In the datasheet there is no such functionality as you already said but when I open the same controller in STM32CubeMX software I found other functions in the same pin and I have also attached the image of that in my previous posts, please go through that and confirm me whether connecting pull down will affect those other peripherals or not?
Regards
Shivakumar
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.