2025-06-09 8:07 AM - edited 2025-06-09 8:11 AM
There's nothing in the manual which tells you which pin is source, and which is load!
PS:
Even the schematic doesn't help!
Solved! Go to Solution.
2025-06-10 2:49 AM
Hello,
There is an ongoing effort to fix this on the newer designs.
Some boards have the pin "1" indication around the IDD jumper, but the schematic forget to tell which one is pin 1...
Some board have "VDD_MCU" marking on one pin, which make it clear.
For that particular board (MB1136), it is an old design, the chances that we roll out an update for that one are low.
Anyways I entered a ticket to add some indication in case it happens:
Internal ticket : #211869
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.