2026-04-03 8:37 AM - last edited on 2026-04-08 2:24 AM by KDJEM.1
Hello Community,
I am struggling with a custom board design based on the STM32H743ZIT6 (LQFP144, non-SMPS version). I’ve replaced the MCU already, but the symptoms remain identical, suggesting a fundamental hardware/layout issue.
The Symptoms:
Current Draw: 10mA when BOOT0 = GND. Approx. 50mA when BOOT0 = 3.3V (System Bootloader).
VCAP Voltage: Measuring approx. 1.0V.
Debug Connection: Using Segger J-Link (V11). "Failed to initialize DAP" / "Can not attach to CPU". VTref is stable at 3.3V, NRST is at 3.3V.
USB DFU: When BOOT0 = 3.3V, Windows reports "Device Descriptor Request Failed" (Unknown Device) when connected via usb.
SWD Pins: PA13/PA14 show ~1.6V when floating (no debugger connected), which is highly unusual
My Schematic:
VBat, all Vdds, Vdda, VRef, PDR_ON are all connected to 3.3V
all GNDs and AGND are connected to GND
each Vcaps (2x) has a 2.2uF capacitor (alltough i am not sure about its esr)
each Vdd pin has its own 100nF or 1uF cap.
=> See stm32schematic.pdf
My Layout:
Vcaps:
As this is a university projekt help would be much appreciated!
Thanks!
Solved! Go to Solution.
2026-04-14 1:35 AM
@QuirinS wrote:
Adding a pullup Resistor to NRST solved the problem.
Thanks for your help!
Hello,
I don't think adding NRST is a solution. Perharps it hides another problem.
There is an internal pull-up resistor inside the chip on NRST pin. See the screenshot from the datasheet posted by @Andrew Neil
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.