2024-01-05 3:56 AM - edited 2024-01-05 4:12 AM
https://drive.google.com/file/d/1r9MhSFT5c7hjDf6kfRWHOomkzLH9iJMF/view?usp=drivesdk Hi Everyone
I made a custom board keeping stm32f429 disc1 board as a reference.
When I connect the the board through usb mini it's showing USB not recognised. Below is my stlink schematic.
Solved! Go to Solution.
2024-01-05 7:59 PM
Well if that is the case You have to replace only chip from st-link part of the board.
2024-01-06 5:52 AM
Sorry for asking it again will my custom board work if I replace STM32F103 chip from my old discovery board and put it into my board what are the precautionary measure before replacing.
Or should I develop fully working code in my disc1 board and replace both chip into my board.
2024-01-06 5:56 AM
I would replace only f103 (programmed chip from st-link), and this board should be able to program via cubeprogrammer or cubeide.
2024-01-06 5:57 AM
If you only replace the STM32F103, it will work. You do not need to change the STM32F4xx chip.
(Provided your board is equivalent to the discovery board.)
2024-01-06 6:27 AM
You can try to program the new STM32F103 to a "selfmade st-link" , see :
https://hackaday.io/project/179054-custom-st-link-v20-v21-v30
2024-01-08 2:17 AM - edited 2024-01-08 4:01 AM
Thank you my board started working like disc1 after replacing STM32F103.
The problem that I'm facing is internal ADC Is giving more noise as compared to disc1 board.
https://drive.google.com/file/d/1rJiLHR7v1m0_u9aUBMIOs7mpG5s_3u-o/view?usp=drivesdk
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.