2019-08-28 1:39 AM
Hello friends.
I want to program my software to STM32H750VBT6.
i Have a st-link v2 usb programmer with SWDIO pin , SWCLK pin ,RST,SWIM and 3.3V & 5V&GND on it,i connected SWDIO ,SWCLK and GND pins to My MicroController.in Debug Of Keil ( Option and target ) I select STM Debuger.Keil Knows Perogrammer But Can't Find Target.
in Last Version Of CubeMX there is a warning which Explains"This ip has no parameters to be configured !!!"---->SystemCore/SYS setting.
i need your helps.
please help me .How i program this chip whit keil??????Thanks.
2019-08-28 2:02 AM
Custom board? Does it work anywhere else, like via STM32 Cube Programmer or ST-LINK Utilities? I'd have NRST wired myself, and be using uVision 5.28a
2019-08-28 2:28 AM
2019-08-28 2:45 AM
Ok, so start by assuming board is nonfunctional, and do basic bring up testing and validation. Start by looking at supplies, idle state of NRST, and VCAP pins.
2019-08-28 2:36 PM
thank you....
i cheked more than 100 times my hardware.
apparently no problem.Vcaps bypassed with 100nF
NRST conected to a pull-up Resistor and bypassed with 100nf.
please send me an empty e-mail i will send back my shematic and software to you.
my mail: Majid_farhangfar@yahoo.com
thank again!!!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.