2026-01-14 9:08 AM - edited 2026-01-17 12:52 PM
Hi, I am trying to move to STM32H750 from STM32F407. To start with I have tried making simple LED blink project and it seems to work.Then I add SDMMC1 and suddenly it started hanging on exiting `static void MX_GPIO_Init(void)`. Any ideas why? Do I need some kind of other initialization or what could be wrong?
/* Identify card operating voltage */
errorstate = SD_PowerON(hsd);
if (errorstate != HAL_SD_ERROR_NONE)
{
hsd->State = HAL_SD_STATE_READY;
hsd->ErrorCode |= errorstate;
return HAL_ERROR;
}
it seems to return error here
0x10000000U
#define SDMMC_ERROR_UNSUPPORTED_FEATURE ((uint32_t)0x10000000U) /*!< Error when feature is not insupported */
what does that mean and how to fix it?
2026-01-17 12:48 PM - edited 2026-01-17 12:51 PM
Inserting SD card worked. but my question is why do we have "Error_Handler();" on "MX_SDMMC1_SD_Init(void)" which is executed if there is no SD card inserted?
static void MX_SDMMC1_SD_Init(void)
{
/* USER CODE BEGIN SDMMC1_Init 0 */
/* USER CODE END SDMMC1_Init 0 */
/* USER CODE BEGIN SDMMC1_Init 1 */
/* USER CODE END SDMMC1_Init 1 */
hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_4B;
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.ClockDiv = 30;
if (HAL_SD_Init(&hsd1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SDMMC1_Init 2 */
/* USER CODE END SDMMC1_Init 2 */
}How do I skip "Error_Handler()" execution if card is not inserted? My board does not have "CardInsert" pin.
Crash if card is not inserted is not what user would expect.
2026-01-19 6:04 AM
Hello @JBond.1
The only possibility is to initialise SDMMC without CubeMX.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.